DOCA0189EN–05

Mounting LC1G115-225 Contactors on Plate

Perform the following procedure to mount the LC1G115-225 contactors on the plate.

  1. Drill 4 holes in the plate. Hole diameter: 4.5 to 6 mm (0.17 to 0.23 in.).

  2. Insert the two short screws (A) diagonally on the plate and tighten the screws with PH2 screwdriver at the right torque.

  3. Place the contactor on the short screw heads.

  4. Insert the two long screws (B) diagonally through the contactor and tighten them at the right torque.

Contactor

Number of poles

G

J

Screws

LC1G115–225

3P

35 mm (1.38 in.)

166 mm (6.53 in.)

M5

4P

70 mm (2.75 in.)

166 mm (6.53 in.)

M5

NOTE: The four screws with nuts and washers are delivered with contactors .
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.