DOCA0189EN–05

Star-Delta Starters

Star-Delta Application Description

Star-delta (or wye-delta) motor starting is used for:

  • motors starting on no-load.

  • motors having a low load torque.

  • motor with load torque increasing with the speed to reduce the stress in the motor and in the distribution network when motor starts.

Examples of this application are fans, compressors with exhaust air and pumps starting with closed valve.

The characteristics of the star-delta starting method are:

  • reduction of the starting current.

  • reduction of the voltage drop.

This method of starting is applicable to three–phase motors on which all six stator terminals are accessible and whose delta connection voltage corresponds to the main voltage. It requires the combination of three contactors. It helps to start the motor with reduced voltage due to the star connection of the stator windings:

  • the starting torque in star connection is reduced to one third of the direct starting torque, that is about 50% of the rated torque.

  • the starting current in star connection is about 1.8–2.6 times the rated current.

The transition from star to delta connection should occur when the machine has run up to its speed. A too rapid build-up in load torque would cause the stabilized run-up speed to be too low and would therefore eliminate any advantage in this method of starting. This is the case with certain machines whose load torque depends on the machine speed (a characteristic of centrifugal machines, for example).

Star-Delta Contactors

The star-delta starter requires the combination of three contactors:

  • The line contactor (L, KM2)

  • The star contactor (Y, KM1)

  • The delta contactor (Δ, KM3)

The line and delta contactors have the same rating and are rated for the motor FLA / √3.

The star contactor is rated for the motor FLA / 3. The size of the star contactor can be

  • the same as the size of the line and delta contactors.

  • the size under the size of the line and delta contactors.

The star and delta contactors must be mechanically and electrically interlocked to avoid short-circuit during transition of the motor stator connections.

The mechanical interlock depends on the type of the three contactors.

Line and delta contactors

Star contactor

Mechanical interlock

Overload relay

LC1G115-225

LC1G115-225

LA9G970

LR9G115–225

LC1G265-500

LC1G265-500

LA9G970

LR9G500

LC1G630-800

LC1G630-800

LA9G973

LR9G630

LC1G265-500

LC1G115-225

LA9G971

LR9G500

LC1G630-800

LC1G265-500

LA9G972

LR9G630

Overload Protection of the Star-Delta Starters

The thermal overload protection of the motor in a star-delta starter can be provided by a TeSys Giga overload relay. The overload relay rating is the same as the rating of the line and delta contactors. The Ir/FLA threshold of the thermal overload protection is set to the motor FLA / √3.

The thermal overload relay can be

  • mounted directly under the line contactor (recommended) or

  • mounted standalone and connected between the motor stator terminals and the delta contactor.

For more information on the star-delta starter power circuit and control circuit diagrams, refer to Power Wiring Diagram and Control Wiring Diagram.

Star-Delta Assembly Video

To access a demonstration video about the assembly of three contactors for a star-delta application, you can click here, scan the QR code, or copy and paste the link to your Web browser.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.