DOCA0189EN–05

Wiring Precautions

Read and understand the following precautions before wiring the devices.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462,NOM 029-STPS or local equivalent.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on this equipment.
  • Use only the specified voltage when operating this equipment and any associated products.
  • Power line circuits must be wired and protected in compliance with local and national regulatory requirements.
  • Beware of potential hazards, and carefully inspect the work area for tools and objects that may have been left inside the equipment.
Failure to follow these instructions will result in death or serious injury.

WARNING
FIRE HAZARD
  • Use only specified wiring cross-section with the equipment and comply with the specified wiring requirements.
  • Tighten the connections to the specified torque values.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

WARNING
UNINTENDED EQUIPMENT OPERATION
Always route low level control wiring and power wiring separately.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.