DOCA0189EN–05

Installation of the Changeover Connection Kits

This section describes the installation procedure of changeover connection kits on the power terminals of the contactors.

  1. Place the coupling bar beside the downstream power terminals of the contactors.

  2. Place the bars to connect the line on the downstream power terminals of one of the contactors.

  3. Insert the screws and washers through the coupling bar and power terminals.

  4. Tighten the screws at the right torque.

Contactor

Tool

Torque

Screws

LC1G115-225

Allen key

18 ± 1.8 N•m (159 ± 15.9 lb-in)

M8

LC1G265-500

Inner hexagon

35 ± 3.5 N•m (310 ± 31 lb-in)

M10

LC1G630-800

Inner hexagon

58 ± 5.8 N•m (513 ± 51.3 lb-in)

M12

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.