DOCA0189EN–05

Removal of Contactor with Cable Memory

The switching modules of advanced contactors or standard contactors with cable memory can be replaced without power disconnection.
Before replacing the switching modules on a contactor with cable memory:
  • Remove the mechanical interlock, if present.

  • Remove all auxiliary contact modules.

Perform the following procedure to remove the contactor with cable memory:

  1. Unscrew the control terminal blocks.
  2. Remove the control terminal blocks.
  3. Remove internal power connection screws cover.
  4. Unscrew with the right tool to remove the internal power connection screws.
  5. Unscrew with an Allen key the four screws fixing the contactor block in the contactor housing.
  6. Remove the contactor block from the contactor housing.

Contactor

Tool

Screws

LC1G115-225

Allen key

M8

LC1G265-500

Inner hexagon

M10

LC1G630-800

Inner hexagon

M12

Contactor

Tool

Length of Allen Key (L)

Screws

LC1G115-225

Allen key

≥ 95 mm (≥ 3.74 in.)

M4

LC1G265-500

Allen key

≥ 115 mm (≥ 4.52 in.)

M4

LC1G630-800

Allen key

≥ 115 mm (≥ 4.52 in.)

M6

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?