IP20 Optional Protection Cover
The IP20 protection cover is an optional protection cover which is used to cover the main power terminals between contactor and overload relay when mounted together.
The table below shows the compatibility of the protection cover with contactors and overload relays:
|
Contactor |
Overload relay |
IP20 cover reference |
|---|---|---|
|
LC1G115-225 |
LR9G115–225 |
LA9G3704 |
|
LC1G265-500 |
LR9G500 |
LA9G3705 |
|
LC1G630-800 |
LR9G630 |
LA9G3706 |