DOCA0189EN–05

Installation of Terminal Shroud with Bars, Lugs or Terminal Extensions

  1. Install the back cover of the terminal shroud on the contactor to lock it automatically with a click.
  2. Place and insert the bars inwards through the back cover of the terminal shroud.
  3. Place and insert the lugs on the power terminals of the contactor.
  4. Insert and tighten the screws at the right torque.
    Contactor

    Type of screws

    Torque

    LC1G115-225

    Allen key

    18±1.8 N•m (159±15.9 lb-in)

    LC1G265-500

    Inner hexagon

    35±3.5 N•m (310±31 lb-in)

    LC1G630-800

    Inner hexagon

    58±5.8 N•m (513±51.3 lb-in)

  5. Install the front cover of the terminal shroud.
  6. Insert and tighten the screws at the right torque to lock the front cover.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.