DOCA0189EN–05

Remote Wear Diagnostic Module

Overview

The remote wear diagnostic module is used for remote signaling of the wear diagnosis function. It can be installed on advanced contactor only.

The module terminals use push-in technology. There are two types of remote wear diagnostic modules depending on the contact arrangement:

  • LA9GRD01: 1 NC contact

  • LA9GRD10: 1 NO contact

Label

Description

A

Plug to the advanced contactor

B

Unlock button

C

Wear signalization contact terminals

D

Wear diagnosis reset button

Reset Button

The Reset button has two functions:

  • If wear diagnosis is detected: switch the Reset button to the left after replacement of the switching modules, to reset the wear diagnosis indication

  • If no wear diagnosis is detected: you can test the control circuit by changing the position of the Reset button. It will change the position of the contact of the module.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.