DOCA0189EN–05

Mounting LC1G265-500 Contactors on Plate

Perform the following procedure to mount the LC1G265-500 contactors on the plate.
  1. Drill 4 holes in the plate. Maximum hole diameter: 6 mm (0.23 in.).

  2. Insert the two short screws (A) diagonally on the plate. The distance between the panel and screw head flat surface shall be between 6 and 14 mm (0.23 and 0.55 in.).

  3. Place the contactor on the short screw heads.

  4. Tighten the two short screws (A) with PZ2 screwdriver at the right torque.

  5. Insert the two long screws (B) diagonally through the contactor and tighten them at the right torque.

Contactor

Number of poles

G

J

Screws

LC1G265–500

3P

45 mm (1.77 in.)

187 mm (7.36 in.)

M5

4P

90 mm (3.54 in.)

187 mm (7.36 in.)

M5

NOTE: The screws with nuts and washers are delivered with contactors .
NOTE: Contactor can also be mounted using four long screws instead of two short screws and two long screws.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.