DOCA0189EN–05

Coding Principle

The commercial reference of Tesys Giga contactors is coded with significant features to explain the type of contactor, current ratings at 440 Vac for AC-3 utilization category, control voltage and number of poles.

Contactors for General Application

NOTE: BEE control voltage option is available on advanced contactors LC1G115-500.

Contactors for Railway Application

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.