DOCA0189EN–05

Overview

The control module contains the components required to control the contactor poles:

  • A fixed magnetic circuit

  • a coil winding

  • an electronic board

There are two types of the control modules:

  • Advanced control module

  • Standard control module

The control module can be replaced by a spare control module after detection of an internal malfunction.

Advanced Control Module

The table below provides the commercial references of the advanced control modules:

Contactor

Control voltage

3P control module

4P control module

LC1G115–225

24–48 Vac/Vdc

LX1G3QBEEA

LX1G4QBEEA

48–130 Vac/Vdc

LX1G3QEHEA

LX1G4QEHEA

200–500 Vac/Vdc

LX1G3QLSEA

LX1G4QLSEA

LC1G265–330

24–48 Vac/Vdc

LX1G3RBEEA

LX1G4RBEEA

48–130 Vac/Vdc

LX1G3REHEA

LX1G4REHEA

200–500 Vac/Vdc

LX1G3RLSEA

LX1G4RLSEA

LC1G400–500

24–48 Vac/Vdc

LX1G3SBEEA

LX1G4SBEEA

48–130 Vac/Vdc

LX1G3SEHEA

LX1G4SEHEA

200–500 Vac/Vdc

LX1G3SLSEA

LX1G4SLSEA

LC1G630–800

48–130 Vac/Vdc

LX1G3TEHEA

LX1G4TEHEA

200–500 Vac/Vdc

LX1G3TLSEA

LX1G4TLSEA

Standard Control Module

The table below provides the commercial references of the standard control modules:

Contactor

Control voltage

3P control module

4P control module

LC1G115–225

48–130 Vac/Vdc

LX1G3QEHEN

LX1G4QEHEN

100–250 Vac/Vdc

LX1G3QKUEN

LX1G4QKUEN

LC1G265–330

48–130 Vac/Vdc

LX1G3REHEN

LX1G4REHEN

100–250 Vac/Vdc

LX1G3RKUEN

LX1G4RKUEN

LC1G400–500

48–130 Vac/Vdc

LX1G3SEHEN

LX1G4SEHEN

100–250 Vac/Vdc

LX1G3SKUEN

LX1G4SKUEN

LC1G630–800

48–130 Vac/Vdc

LX1G3TEHEN

LX1G4TEHEN

100–250 Vac/Vdc

LX1G3TKUEN

LX1G4TKUEN

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.