DOCA0189EN–05

Overload Relay Wiring Characteristics

The table below provides wiring characteristics of the push-in terminals blocks of overload relays:

Cable type

Stripping length

Number of conductors

Section

Solid Cable

10 mm (0.40 in.)

1 conductor without cable end

0.2–2.5 mm²

(26–14 AWG)

2 conductors with suitable dual sleeve

0.5-1.0 mm²

(20-18 AWG)

Flexible cable

10 mm (0.40 in.)

1 conductor with suitable cable end or sleeve

0.2–2.5 mm²

(26–14 AWG)

2 conductors with suitable dual sleeve

0.5-1.0 mm²

(20-18 AWG)

Do not use flexible cable without cable end or sleeve.

For the overload relay wiring diagram, see Wiring Diagram.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.