DOCA0189EN–05

Coding Principle

The commercial reference of TeSys Giga overload relays is coded with significant features to explain the type and the ratings of the overload relay.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?