DOCA0189EN–05

Thermal Dissipation

This section describes the thermal dissipation characteristics for the contactors and control modules, and thermal overload relays.

Main Power Lines of Contactors

Contactor

Power dissipation per pole at maximum current with AC–1 load

Power dissipation per pole at maximum current with AC–3/AC–3e load

LC1G115

9 W

2 W

LC1G150

11 W

3 W

LC1G185

14 W

5 W

LC1G225

16 W

8 W

LC1G265

40 W

19 W

LC1G330

52 W

29 W

LC1G400

61 W

32 W

LC1G500

98 W

50 W

LC1G630

88 W

32 W

LC1G800

88 W

51 W

Contactors Control Modules

Contactor

Heat dissipation for standard control module

Heat dissipation for advanced control module

LC1G115–225

5–6 W

4–5 W

LC1G225–330

6–7 W

5–6 W

LC1G400–500

6–7 W

5–6 W

LC1G630–800

6–7 W

5–6 W

Overload Relays

Overload relay

Maximum heat dissipation at Ir Max

LR9G115

1 W

LR9G225

3 W

LR9G500

5 W

LR9G630

8 W

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.