DOCA0189EN–05

Power Wiring Diagram

NOTICE
HIGH TRANSIENT CURRENT
Follow scrupulously the wiring diagram and phase sequence.
Failure to follow can result in high transient current when switching from star to delta connection.

Star-delta motor starter with thermal magnetic circuit breaker and contactors

Star-delta motor starter with magnetic circuit breaker, overload relay, and contactors

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?