DOCA0189EN–05

Installation of Terminal Shroud with Coupling Bars

With coupling bars, the back cover of the terminal shroud cannot be installed. You can use optional lug covers LA9G3707 or LA9G4707 to improve insulation of the coupling bars.
  1. Place and insert the coupling bars on the power terminals of the contactor.
  2. Place and insert the lugs inwards on the power terminals of the contactor.
  3. Insert and tighten the screws at the right torque.

    Contactor

    Type of screws

    Torque

    LC1G115-225

    Allen key

    18±1.8 N•m (159±15.9 lb-in)

    LC1G265-500

    Inner hexagon

    35±3.5 N•m (310±31 lb-in)

    LC1G630-800

    Inner hexagon

    58±5.8 N•m (513±51.3 lb-in)

  4. Install the front cover of the terminal shroud.
  5. Insert and tighten the screws at the right torque to lock the front cover.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?