DOCA0189EN–05

TeSys Giga Contactor Mounting on Retrofit Base

Overview

Retrofit bases are designed for integrating TeSys Giga contactors into installations using TeSys F contactors. The retrofit bases help reduce replacement and reinstallation time when you upgrade your system with the new range of TeSys Giga contactors . The bases come in three frame sizes.

Contactor

Retrofit base

LC1G115–225

LA9GRFB1

LC1G265-500

LA9GRFB2

LC1G630-800

LA9GRFB3

Mounting Dimensions

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.