Diagnosis LED
The below table provides the different LED indication functions:
|
LED indication |
Diagnosis indication |
Diagnosis function |
|
The contacts are worn, see Diagnosis Functions |
Diagnosis contact wear |
|
|
The control voltage is lower than 80 % of Ucmin, see Diagnosis Functions |
Under voltage |
|
|
The control voltage is higher than 110 % of Ucmax, see Diagnosis Functions |
Over voltage |
|
|
The remote wear diagnosis module is not synchronized with the contactor, see Diagnosis Functions |
Remote wear diagnosis module synchronization |
|
|
The wear diagnosis reset is in progress, see Switching Module Replacement |
Reset of remote wear diagnosis |
|
|
A control module internal malfunction is detected, see Troubleshooting |
Internal functioning |