Abandon Model Names and Settings

Below are the model names and Abandon tab settings that must be assigned to configure Abandon for Gas, Water, and Electric geodatabases. All model names, field model names, and settings are assigned using the ArcFM Properties Manager. Model names are assigned on the Model Names tab and field model names on the Field Model Names tab. Settings are made on the Abandon Info tab.

The feature classes shown are those used in the Minerville sample geodatabase. Use the equivalent feature classes in your geodatabase. Assign all field model names to the appropriate fields.

Gas Abandon

AbandonedRemovedGasDevice

Model Names

MMREMOVED, MMREMOVABLE

Field Model Names

AT_MATERIAL, AT_MODEL, AT_MANUFACTURER, AT_VALVESIZE, AT_VALVETYPE

AbandonedRemovedGasPipe

Model Names

MMREMOVED

Field Model Names

AT_MANUFACTURER, AT_MATERIAL, AT_PIPESIZE

AbandonedGasDevice

Model Names

MMABANDONED, MMREMOVABLE

Field Model Names

AT_MANUFACTURER, AT_MODEL, AT_VALVESIZE, AT_VALVETYPE, AT_MATERIAL

Abandon Info Settings

Set On Abandon and Remove To AbandonedRemovedGasDevice.

AbandonedGasPipe

Model Names

MMABANDONED, MMREMOVABLE

Field Model Names

Assign the field model name MMCONDUITINDICATOR to the ConduitIndicator field. Assign the field model names AT_MATERIAL, AT_PIPESIZE, and AT_MANUFACTURER to the appropriate fields.

Abandon Info Settings

Set On Abandon and Remove To AbandonedRemovedGasPipe.

DistributionMain

Model Names

MMABANDONABLE, MMCONDUITABLE, MMREMOVABLE

Field Model Names

AT_PIPESIZE, AT_MATERIAL, AT_MANUFACTURER

Abandon Info Settings

Set Abandon To AbandonedGasPipe. Set Abandon and Remove To AbandonedRemovedGasPipe.

Service

Model Names

MMABANDONABLE, MMCONDUITABLE

Field Model Names

AT_PIPESIZE, AT_MATERIAL, AT_MANUFACTURER

Abandon Info Settings

Set Abandon To AbandonedGasPipe. Set Abandon and Remove To AbandonedRemovedGasPipe.

GasValve

Model Names

MMABANDONABLE, VALVE

Field Model Names

AT_MANUFACTURER, AT_VALVESIZE, AT_VALVETYPE, AT_MODEL, AT_MATERIAL

Abandon Info Settings

Set On Abandon To AbandonedGasDevice. Set On Abandon and Remove To AbandonedRemovedGasDevice.

Water Abandon

AbandonedRemovedWaterDevice

Model Names

MMREMOVED

Field Model Names

AT_MATERIAL, AT_MODEL, AT_MANUFACTURER, AT_VALVESIZE, AT_VALVETYPE

AbandonedRemovedWaterPipe

Model Names

MMREMOVED

Field Model Names

AT_MANUFACTURER, AT_MATERIAL, AT_PIPESIZE

AbandonedWaterDevice

Model Names

MMABANDONED, MMREMOVABLE

Field Model Names

AT_MANUFACTURER, AT_MODEL, AT_VALVESIZE, AT_VALVETYPE, AT_MATERIAL

Abandon Info Settings

Set On Abandon and Remove To AbandonedRemovedWaterDevice.

AbandonedWaterPipe

Model Names

MMABANDONED, MMREMOVABLE

Field Model Names

Assign the field model name MMCONDUITINDICATOR to the ConduitIndicator field. Assign the field model names AT_MATERIAL, AT_PIPESIZE, and AT_MANUFACTURER to the appropriate fields.

Abandon Info Settings

Set On Abandon and Remove To AbandonedRemovedWaterPipe.

GravityMain

Model Names

MMABANDONABLE, MMCONDUITABLE, MMREMOVABLE

Field Model Names

AT_MATERIAL, AT_MANUFACTURER, AT_NOMINALDIAMETER

Abandon Info Settings

Set Abandon To AbandonedWaterPipe. Set Abandon and Remove To AbandonedRemovedWaterPipe.

LateralLine

Model Names

MMABANDONABLE, MMCONDUITABLE

Field Model Names

AT_PIPESIZE, AT_MATERIAL, AT_MANUFACTURER

Abandon Info Settings

Set Abandon To AbandonedPipe. Set Abandon and Remove To AbandonedRemovedWaterPipe.

SystemValve

Model Names

MMABANDONABLE, MMREMOVABLE, VALVE

Field Model Names

AT_MANUFACTURER, AT_VALVESIZE, AT_VALVETYPE, AT_MODEL, AT_MATERIAL

Abandon Info Settings

Set On Abandon To AbandonedWaterDevice. Set On Abandon and Remove To AbandonedRemovedWaterDevice.

Electric Abandon

Object class that represents abandoned removed conductor

Model Names

MMABANDONRELATE, MMREMOVED

Field Model Names

Assign field model name AT_(field name) to any field that will have values transferred from source to destination class.

AbandonedRemovedDevice object class

Model Names

MMREMOVED

Field Model Names

Assign field model name AT_(field name) to any field that will have values transferred from source to destination class.

Feature class that represents conductors abandoned in place

Model Names

MMABANDONED, MMREMOVABLE, MMABANDONRELATE (if conductors are represented as a bank/unit relationship)

Field Model Names

Assign field model name AT_(field name) to any field that will have values transferred from source to destination class.

Abandon Info Settings

Set Abandon and Remove To: object class that represents conductors that have been abandoned and removed.

Feature classes that represent electric devices that have been abandoned in place; may have one feature class to hold all devices or one for each device

Model Names

MMABANDONED, MMREMOVABLE

Field Model Names

Assign field model name AT_(field name) to any field that will have values transferred from source to destination class.

Abandon Info Settings

Set Abandon and remove to: object class that represents electric device that has been abandoned and removed.

Any electric device for which you want to maintain information after it has been abandoned in place or abandoned and removed

Model Names

MMABANDONABLE, MMREMOVABLE

Field Model Names

Assign field model name AT_(field name) to any field that will have values transferred from source to destination class.

Abandon Info Settings

Set Abandon to: feature class that represents abandoned device and Abandon and remove to: object class that represents abandoned and removed device.

Any Conductor

Model Names

MMABANDONABLE, MMREMOVABLE, MMABANDONRELATE (if conductors are represented as a bank/unit relationship)

Field Model Names

Assign field model name AT_(field name) to any field that will have values transferred from source to destination class.

Abandon Info Settings

Set Abandon to: feature class representing abandoned conductor; set Abandon and remove to: object class representing abandoned and removed conductor; set On Abandon to: Unrelate and Re-relate.

To abandon to a subtype of the conductor feature class, add the subtype, then on the Abandon Info tab, select the subtype you want to abandon; set Abandon To: Abandoned subtype.

If you want to change the value of an indicator field when a conductor is abandoned, add a field called AbandonedIndicator, type Text, Default Value N, and Domain Yes/No Indicator.

Set Abandon and remove to: Abandoned and Removed Conductor and On Abandon: Change AbandonedIndicator field.

ConductorInfo object class

Model Names

MMABANDONRELATE (if conductors are represented as a bank/unit relationship)

Field Model Names

Assign field model name AT_CONDUCTORMATERIAL to Conductor Material field. Assign field model name AT_CONDUCTORSIZE to Conductor Size field. Assign field model name AT_PHASEDESIGNATION to Phase Designation field.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.