Effective Coefficient of Friction

The effective coefficient of friction for a multiple cable pull is a function of the basic coefficient of friction KQ and the weight correction factor Wc.

This increase in friction (K) is caused by an increase in the weight correction factor (Wc). The Wc accounts for the wedging action between the cables and the conduit. The following equation calculates the effective coefficient of friction:

K = KQ Wc

Where:

K = Effective coefficient of friction (dimensionless)

KQ = Basic coefficient of friction (dimensionless)

Wc = Weight correction factor (dimensionless)

Research data indicates that at a sidewall bearing pressure (SWBP) of approximately 150 Ib/ft or more, the effective coefficient of friction is significantly reduced. In effect, this means that when the cable is pulled around bends, initially use the higher coefficient of friction to calculate the SWBP. When the SWBP is greater than or equal to 150 Ib/ft, use the lower coefficient of friction.

Table: Basic Coefficients of Friction - KQ

Type of Conduit

Cable Outer Covering Material

Bends where SWBP is < 150 lb/ft and Straight Pulls

Bends where SWBP exceeds 150 lb/ft

Single Cable Pull

Multiple Cable Pull

PVC

XLP, 600V

concentric wires

PE jacket

PVC jacket

Neoprene

.40

.40

.40

.50

.90

.60

.40

.45

.60

1.50

.15

.20

.15

.30

.15

Steel

XLP, 600V

concentric wires

PE jacket

PVC jacket

Neoprene

.60

.50

.50

.65

1.05

.65

.50

.50

.65

1.75

.25

.30

.25

.30

.25

Bitumenized Fiber

XLP, 600V

concentric wires

PE jacket

PVC jacket

Neoprene

.30

.40

.25

.40

.40

.65

.40

.60

.45

.55

--

--

--

--

--

Terra-Cotta or Transite

XLP, 600V

concentric wires

PE jacket

PVC jacket

Neoprene

.70

--

.70

.70

1.00

.70

--

.70

.70

1.80

--

--

--

--

--

Fiberglass

XLP, 600V

PE jacket

PVC jacket

Neoprene

.23

.25

.39

.53

.23

.25

.39

.53

.15

.15

.30

.15

PE

XLP, 600V

concentric wires

PE jacket

PVC jacket

Neoprene

CN

.45

.20

.25

.30

.65

.20

.55

.20

.85

.45

.65

.15

.20

.15

.30

.15

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.