Customer and Service Overview

Residential, commercial, and industrial customers and resellers, as well as special devices such as streetlights, constitute the loads on the electrical system. Simple junction features are the electric locations (for example, primary meters and service points). Objects contain customer information and information about generators of alternate sources of electricity. Primary meters, delivery points, and generators may be associated with a structure.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.