Aerial Marker

An AerialMarker indicates the presence of overhead cable and structures. AerialMarker inherits attributes from the Structure abstract class.

Subtypes: None

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

LightIndicator

text

Code indicating presence of light indicator; domain values or Yes and No.

SymbolRotation

double

Angle of rotation indicating how a feature appears on the map. Uses the SYMBOLROTATION model name. The ArcFM Manual Angle Setter edit task and ArcFM Auto Angle Setter autoupdater both use this field to rotate point features.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.