Designer Field Model Names

Model Name

Attribute

DESIGNID

DesignID attribute in all Feature Classes

WORKFLOWSTATUS

WorkFlowStatus attribute in all Feature Classes

WORKFUNCTION

WorkFunction attribute in all Feature Classes

WORKLOCATIONID

WorkLocationID attribute in all Feature Classes

WORKREQUESTID

WorkRequestID attribute in all Feature Classes

Designer Non-Creatable Features

Model Name

Object

DESIGN

The Design Feature class in the Designer Dataset; prevents this feature class from displaying in the CU tab.

WORKLOCATION

The WorkLocation Feature class in the Designer Dataset; prevents this feature class from displaying in the CU tab.

WORKREQUEST

The WorkRequest Feature class in the Designer Dataset; prevents this feature class from displaying in the CU tab.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.