Joint Use Attachment

Other utilities or entities may attach conductors or cables that carry signals such as community antenna television systems (CATV) to support structures. Information about owners and joint use attachments is captured in this table. This related object class stores information about a feature with a spatial reference but does not itself have a location on the map.

Structural Analysis (in Designer) uses this object class when performing "what if" simulations to evaluate the structural integrity of a support structure and its associated features.

Subtypes: None

Associations: SupportStructure

Model Names: JOINTUSEATTACHMENT

Attributes:

Field Name

Field Type

Description

AttachmentDate

date

Date object was attached to structure. Uses DATE model name on this field.

AttachmentHeight

text

The height of the attachment. This value should be expressed in the same units used for the SupportStructure Height field.

AttachmentType

text

The type of attachment.

Chargeable

text

A boolean value that indicates whether the attachment is chargeable.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

Owner

text

Code indicating owner of attachment; domain values include Cable, Telephone, Other, etc. Structural Analysis uses the JOINTUSEATTACHMENTOWNER model name on this field.

StructureObjectID

long integer

Object ID for the structure.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.