GasMeter

Accurate measurement of volume of gas flowing in pipelines is crucial to well analysis and loss prevention. Meter types include diaphragm, orifice, and rotary.

Subtypes: None

Associations: MeterSetting, RuralTap, TownBorderStation

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

FlowCapacity

text

Rated capacity in cubic feet per minute (cfm).

MeterMAOP

double

Maximum allowable operating pressure of meter.

MeterSettingObjectID

long integer

ObjectID of associated MeterSetting.

MeterType

text

Code indicating meter type; domain values include Diaphragm, Orifice, and Rotary.

Owner

text

Owner of Meter.

PressureRating

text

Pressure across meter in psi.

PropertyUnitCode

text

Value assigned to assets to track and classify Property Records.

RecordingMethod

text

Time recording method to calculate volume.

RuralTapObjectID

long integer

ObjectID of associated RuralTap.

SerialNumber

text

Serial number of meter.

TBSObjectID

long integer

Object ID of associated town border station.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.