XML

The XML folder contains .dtd and .xsd files that verify the XML imported and exported by ArcFM. These files are found in the Program Files\Miner and Miner\ArcFM Solution\Bin\XML folder of the ArcFM Solution installation directory.

IMPORTANT: DO NOT MOVE OR RENAME THE FILES IN THIS DIRECTORY.

File Name

Description

Used by Tools:

CU.dtd

Validates the structure of CUs and GUs upon import.

Designer

CymdistImport.dtd

Validates the XML exported from the geodatabase to ensure it is the proper structure before passing it to the CYMDIST API.

Network Adapter

DatabaseConnections.xml

Stores connection information for ArcFM Viewer for ArcGIS Engine. Access this information using the ArcFM Engine Administrator.

ArcFM Engine Administrator

DatabaseProperties.dtd

Validates the XML used by the Import/Export tool when importing or exporting database properties.

XML Import/Export Tool

Design.dtd

Validates the structure of the design.

Designer

DesignOptimizationLayerSymbology.xml

A sample file of Design Optimization symbology layers in XML format.

Designer

domains.dtd

Validates the XML used by the Import/Export tool when importing or exporting domain information.

XML Import/Export Tool

FeatureClass.dtd

Validates the XML used by the Import/Export tool when importing or exporting feature class information.

XML Import/Export Tool

FimObject.dtd

Validates the XML used by the Import/Export tool when importing or exporting ArcFM properties information.

XML Import/Export Tool

GeometricNetwork.dtd

Validates the XML used by the Import/Export tool when importing or exporting geometric network information.

XML Import/Export Tool

GraphicsFavorites.dtd

Validates the XML used to import graphic favorites.

Graphics Tab

GxXML.dtd

This .dtd wraps several other .dtds: Featureclass.dtd, Snapping.dtd, ModelNames.dtd, Domains.dtd, ObjectInfo.dtd, RelationshipClass.dtd, GeometricNetwork.dtd, and DatabaseProperties.dtd.

XML Import/Export Tool

Miner.layout.xsd

Validates the XML used by the Custom Layout File.

ArcFM Viewer for ArcGIS Engine

MinervilleCymdistEquipment.xml

Contains substation, generator, and motor equipment for the Minerville sample data. This equipment must be imported into CYMDIST before feeders can be exported from the Minerville sample data.

Network Adapter

modelnames.dtd

Validates the XML used by the Import/Export tool when importing or exporting model name information.

XML Import/Export Tool

MspDefaults.xml

Contains the default values for the MultiSpeak export for null fields.

 

mspGeometry.xsd

Contains definitions from the GML standard. This file is from the MultiSpeak consortium.

Network Adapter

Multispeak.xsd

Defines features and attributes in the MultiSpeak specification. This file is from the MultiSpeak consortium.

Network Adapter

MultispeakRealTime.xsd

Defines the message header information. It is used to validate MultiSpeak XML and references MultiSpeak.xsd and mspGeometry.xsd. This file is from the MultiSpeak consortium.

Network Adapter

NetworkAdapterGML.dtd

Contains definitions for geometry in GML format.

Network Adapter

NetworkAdapterNetwork.dtd

Validates the XML exported from the geodatabase to ensure it is the proper structure before passing it to the Vendor API.

Network Adapter

NetworkAdapterNetworkSample.xml

The file provides sample XML that has been exported from a geodatabase and is ready to be passed to the Vendor API.

Network Adapter

NetworkAdapterResults.dtd

Validates the XML used to import analysis results to the Analysis API.

Network Adapter

NetworkAdapterResultsSample.xml

This file provides sample analysis results in XML format.

Network Adapter

NetworkAdapterTestCase.dtd

Used for load cases.

Network Adapter

NetworkAdapterTestCaseSample.xml

This file provides a sample load case in XML format.

Network Adapter

ObjectInfo.dtd

Validates the XML used by the Import/Export tool when importing or exporting class extenion type and geo-object information.

XML Import/Export Tool

PxUsers.dtd

Validates the XML used by the Process Framework Administration Tool when importing or exporting user information on the Import/Export tab.

Process Framework Administration tool

PxWorkflow.dtd

Validates the XML used by the Process Framework Administration Tool when importing or exporting a Process Framework workflow on the Import/Export tab.

Process Framework Administration tool (Designer/Workflow Manager only)

PxXML.dtd

This .dtd wraps two .dtds: PxWorkflow.dtd and WorkflowManagerCU.dtd.

Process Framework Import/Export tool

QAQC.dtd

Validates the XML used by the QA/QC tool when the user elects to Write to File or Write All to File.

QA/QC

RelationshipClass.dtd

Validates the XML used by the Import/Export tool when importing or exporting relationship class information.

XML Import/Export Tool

Sample.ArcFMViewer.exe.layout

This is a sample copy of the custom laytout file used to distribute user interface customizations to ArcFM Viewer for ArcGIS Engine.

ArcFM Viewer for ArcGIS Engine

snapping.dtd

Validates the XML used by the Import/Export tool when importing or exporting snapping information.

XML Import/Export Tool

WorkflowManagerCU.dtd

Validates the XML used by the Process Framework Administration Tool when importing or exporting Compatible Units on the Import/Export tab.

Process Framework Administration tool (Designer/Workflow Manager only)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.