ElectricSurvey

Electric surveys are completed periodically above ground where metal pipes are located to monitor how fast they are corroding.

Subtypes: None

Associations: Drip, LeakReport, PipeExposure

Model Names: None

Attributes:

Field Name

Field Type

Description

Amperage

text

System rated capacity of rectifier in amps.

Comments

text

User or designer comments.

DistributionMainObjectID

long integer

ObjectID of associated Distribution Main.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

ServiceObjectID

long integer

ObjectID of associated Service GasPipe.

SurveyDate

date

Date of last Electric Survey.

SurveyDueDate

date

Date next Electric Survey is due to be performed.

SurveyFrequency

text

Frequency of Electric Survey.

Voltage

long integer

Amount of voltage output by rectifier in amps.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.