Scrubber

Like a strainer, this device is used to remove or “scrub” foreign materials from natural gas (e.g., dust, dirt).

Subtypes: None

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InstallationDate

date

Date of installation.

Owner

text

Owner of scrubber.

PropertyUnitCode

text

Value assigned to assets to track and classify Property Records.

SymbolRotation

double

Angle that indicates how the feature appears on a map.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.