Network Adapter Field Model Names

Model Name

Object

CYMDISTEXPORT

Any attribute on a feature class that should be exported for use with the Electric Analysis engine provided by Cyme

MSPKVARA

KVAR on phase A

MSPKVARB

KVAR on phase B

MSPKVARC

KVAR on phase C

MSPKWA

Kilowatts on phase A

MSPKWB

Kilowatts on phase B

MSPKWC

Kilowatts on phase C

MSPLOADCASE

Denotes the name of the load case. This field is used to distinguish between multiple load values relating to the same feature. For example, you may store both winter peak and summer peak load values in the LoadCase table. You can do this by assigning a different load name to each record. "Winter Peak", and "Summer Peak", for example.

MSPLOADFOREIGNKEY

A unique ID for network features that have related load data. This field is used as a key between the LoadCase table and the network feature class that it is related to (typically TransformerBank or ServiceLocation), and it should be assigned to the key field in both the LoadCase table and the feature class.

SYNERGEE_CONFIGURATION1

Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs.

SYNERGEE_CONFIGURATION2

Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs.

SYNERGEE_EQUIP1

Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs.

SYNERGEE_EQUIP2

Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs.

SYNERGEE_MANUFACTURER1

Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs.

SYNERGEE_MANUFACTURER2

Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs.

SYNERGEE_MECHANICALRESPONSE1

Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs.

SYNERGEE_MECHANICALRESPONSE2

Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs.

SYNERGEE_MODEL1

Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs.

SYNERGEE_MODEL2

Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs.

SYNERGEE_NEUTRALCONDUCTOR1

Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs.

SYNERGEE_NEUTRALCONDUCTOR2

Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs.

SYNERGEE_PHASECONDUCTOR1

Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs.

SYNERGEE_PHASECONDUCTOR2

Used to identify attributes that make up the Equipment ID. This is discussed in depth in the Network Adapter Implementation Guide, Electric Solver Equipment IDs.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.