CPBondWire

Bond wire connects two nonadjacent sections of pipe to maintain the pipe in a “cathodic” state. CPBondWire is considered a simple edge feature because it is connected to other devices only at its ends and is used to perform traces to test the cathodic protection system.

You may omit specific feature classes from gas traces. To do this, assign the GASNONTRACABLE model name to the CPBondWire feature class. The GASNETWORKEDGE model name is used to configure gas tracing in ArcFM Viewer for ArcGIS Engine. Assign to all Gas Network Edge feature classes that participate in gas tracing

Subtypes: None

Associations: CPBondJunction, CPSystem

Model Names: GASNETWORKEDGE, GASNONTRACABLE

Attributes:

Field Name

Field Type

Description

Color

text

Color assigned to CPSection; domain values include Aqua, Forest, and Pink.

Comments

text

Comments of user or designer.

CPSystemObjectID

long integer

Object ID of associated system.

Depth

double

Depth of CPBondWire.

GasTraceWeight

long integer

Information used for tracing analysis; stored in a bitgate. Gas tracing uses the GASTRACEWEIGHT model name on this field.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InServiceDate

date

Date bond wire was set in service.

InstallationDate

date

Date bond wire was installed.

LengthSource

text

Source of length measurement; domain values are Mapping System and Field Measurement.

LocationDescription

text

Verbal description of location of bond wire.

Material

text

Code indicating material of wire.

MeasuredLength

double

Field-measured length of CPBondWire, ranging from 1 to 1,000,000,000. Gas tracing uses the MEASUREDLENGTH model name on this field.

OperatingStatus

text

Code indicating functional status of CPBondWire; domain values include Active, Designed, and Proposed Retire.

PropertyUnitCode

text

Value assigned to assets to track and classify.

WireDiameter

text

Diameter of CPBondWire.

WireSize

text

Size of CPBondWire.

WorkOrderID

text

Utility-defined identifier of work order.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.