CPRectifier

A rectifier is the source of direct current in the cathodic protection system. Wire connects the pipe to the negative pole of the rectifier. The positive pole is connected to the ground bed that contains anodes. Current flows from the rectifier through the ground bed, through the soil to the pipe, and back to the rectifier. The ground bed deteriorates over time, but the pipe is protected.

You may omit specific feature classes from gas traces. To do this, assign the GASNONTRACABLE model name to the CPRectifier feature class. A rectifier bit depends on the existence of the class model name RECTIFIER. LOCATABLEOBJECT is used to enable the Object Query Locator tool.

CPRectifier acquires properties from the CathodicProtectionDevice abstract class.

Subtypes: None

Associations: None

Model Names: GASNONTRACABLE, RECTIFIER

Attributes:

Field Name

Field Type

Description

Amperage

text

System rated capacity of rectifier in amps.

CoolingMethod

text

Code indicating cooling method of rectifier; domain values include air or oil.

CPSystemObjectID

long integer

ObjectID of associated CPSystem.

FacilityID

text

Utility identifier representing a feature’s location in the facility; if the feature is replaced, the new feature has the same identifier. Assign the LOCATABLEFIELD model name to enable this field for the Object Query Locator tool. The feature or object class must have the model name LOCATABLEOBJECT assigned.

InternalMeter

text

Code indicating presence of InternalMeter; domain values are Yes or No.

Manufacturer

text

Code indicating manufacturer; domain values include Goodall, Kerotest, Rockwell, etc. The AT_MANUFACATURER model name is used on this field to configure abandon for gas.

Model

text

Rectifier model number specified by manufacturer.

RectifierType

text

Code indicating type of rectifier; domain values include CPRectifier - General, RectifierBond, Rectifier.

SerialNumber

text

Rectifier serial number specified by manufacturer. Assign the LOCATABLEFIELD model name to enable this field for the Object Query Locator tool. The feature or object class must have the model name LOCATABLEOBJECT assigned.

Voltage

long integer

Amount of voltage output by rectifier in amps.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.