CPSystem

IMPORTANT: This class has been superceded by a new Cathodic Protection System data model as of ArcFM Solution 10.0.3. If you currently use this class to group gas network features by CP system, you may continue to do so. If you intend to begin modeling CP systems or want to use the new CP data model, view the ArcFM Desktop Configuration Guide topics under the Gas Tracing heading.

A CPSystem is composed of multiple pipe sections and defined for the purpose of performing cathodic protection trace analysis.

Subtypes: None

Associations: CPBondWire, CPDevice, GasPipe

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

ID

text

Primary key for utility identifier.

ProtectionType

text

Type of protection used in system; includes Anode and Rectified.The PROTECTIONTYPE model name is assigned to this field for gas tracing operations.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.