Unit Object

UnitObject is an abstract class containing common attributes of individual devices: capacitors, fuses, reclosers, sectionalizers, switches, and transformers.

Associations: None

Subtypes: None

Model Names: None

Attributes:

Field Name

Field Type

Description

PhaseDesignation

long integer

Code indicating phases present; domain values include A, AB, AC, etc. Feeder Manager and Electric Tracing require the PHASEDESIGNATION model name on this field.

UnitID

text

Identifier of related device unit.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.