ArcFM Feeder Cache Maintenance Autoupdater

The ArcFM Feeder Cache Maintenance Autoupdater is an AU that is automatically assigned when you turn on Feeder Manager 2.0 in ArcCatalog. This also means if you turn Feeder Manager 2.0 off the Feeder Cache Maintenance AU is turned off.

The Feeder Cache Maintenance Autoupdater is assigned to events on each feature class in the geometric network. It is also assigned to events on the CircuitSource and Subsource tables, as well as the relationship class that joins the circuit source feature class (e.g. DynProtDevice) to the CircuitSource table.

The assignments associated with the Feeder Cache Maintenance AU are described below so you know that to expect when examining Autoupdater assignments to the listed feature class and event types

All feature classes in the geometric network, including the default junction feature class:

  • On Feature Create

  • On Feature Update

  • On Feature Delete

All edge feature classes in the electric geometric network:

  • Before Feature Split

  • On Feature Split ( required for simple edge feature classes)

  • After Feature Split

The CircuitSource table:

  • On Feature Update

The Subsource table (commonly named CircuitSourceID):

  • On Feature Update

The relationship class that joins the circuit source feature class (e.g. DynProtDev) to the CircuitSource table:

  • On Relationship Created

  • On Relationship Deleted

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.