Odorizer

Because natural gas is odorless and colorless, odorizers are used for leak detection at or near the gas point of purchase. Odorizer delivery methods are based on the size of the system, flow, and electrical power available.

Assign the LOCATABLEOBJECT model name to enable fields for the Object Query Locator tool.

Subtypes: Bypass, Injection Pump, Pulse, RuralTap, Wick

Associations: RuralTap

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

GasTraceWeight

long integer

Information used for tracing analysis; stored in a bitgate. Gas Tracing uses the GASTRACEWEIGHT model name.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InstallationDate

date

Date of installation.

Manufacturer

text

Manufacturer of Odorizer; domain values include King Tool, Williams Pump, YZ Industries, etc.

Owner

text

Owner of Odorizer.

PropertyUnitCode

text

Value assigned to assets to track and classify Property Records.

RuralTapObjectID

long integer

Object ID of associated RuralTap.

SerialNumber

text

Serial Number of Odorizer. Assign the LOCATABLEFIELD model name to enable fields for the Object Query Locator tool. The feature or object class must have the model name LOCATABLEOBJECT assigned.

StorageCapacity

text

Amount Odorizer is able to store; domain values include 250#, above ground, .1cc, unknown, etc.

SymbolRotation

double

Angle that dictates how the feature appears on the map.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.