Fuse Unit

A fuse is an intentionally weakened spot in the electric circuit that opens the circuit at a predetermined current that is maintained for a predetermined amount of time. Fuses are classified into three categories: low voltage (through 600 V), medium voltage (operating through 69 kV) and high voltage (through 500 kV).

Designer uses the DESIGNUNIT model name on this class to designate it as an electric device unit object class. The Designer Work Function Tool uses this model name to identify all electric device unit object classes.

Associations: Fuse

Subtypes: None

Model Names: DESIGNUNIT

Attributes:

Field Name

Field Type

Description

FuseObjectID

long integer

ObjectID of associated Fuse.

HousingType

text

Code indicating type of FuseUnit housing; domain values include Door Cutout, MX Cutout, and Open Link.

HousingRating

long integer

Code indicating capacity of FuseUnit housing in amps; domain values include 50 amps, 100 amps, 200 amps, etc.

LinkType

text

Code indicating type of FuseUnit link, in terms of speed; domain values include KLink, NLink, 200, etc.

LinkRating

long integer

Size of FuseUnit link in amps; domain values include 1 A, 10 A, 100 A, etc.

Manufacturer

text

Code indicating manufacturer.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.