LeakReport

Leak reports represent areas on pipes where leaks have been detected. A Leak Report can be associated with any applicable</p>e gas facility (e.g., valves or fittings).

LEAKREPORT is used for gas model configuration. LOCATABLEOBJECT is used to enable the Object Query Locator tool.

Subtypes: None

Associations: GasPipe, LeakRepair

Model Names:  LEAKREPORT

Attributes:

Field Name

Field Type

Description

Address

text

Address location of reported leak.

ClosedDate

date

Date leak report closed.

ClosedStatus

text

Code indicating leak closed status; domain values include Active, Cleared, and Repaired.

Comments

text

User and designer comments.

CurrentLeakClass

text

Code indicating current leak class; domain values include Class 1, Class 2, etc.

DateReported

date

Date leak was reported.

DistributionMainObjectID

long integer

ObjectID of associated DistributionMain.

DOTReportedIndicator

text

Indicates whether leak is reported to DOT; domain values are Yes and No.

FederalLandIndicator

text

Indicates whether leak is located on federal land; domain values are Yes and No.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InstallationDate

date

Date of installation.

LastCheckDate

date

Date of last leak check.

LeakID

text

Utility-defined identifier of leak. Assign the LOCATABLE field model name to enable fields for the Object Query Locator tool. The feature or object class must have the model name LOCATABLEOBJECT assigned.

LeakSurveyType

text

Type of survey program used to detect leak; domain values include Aerial, Mobile Truck, and Walking.

NextCheckDate

date

Date of next check.

OriginalLeakClass

text

Code indicating original leak classification; domain values include Class 1, Class 2, etc.

ServiceObjectID

long integer

ObjectID of associated service pipe.

SoilType

text

Type of soil in which pipe is buried; domain values include Clay, Rock, Sand, Other, and Unknown.

SurfaceType

text

Code indicating ground surface type; domain values include Concrete, Grass, Gravel, Other, and Unknown.

SymbolRotation

double

Angle that dictates how the feature appears on map.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.