GasStation

GasStation is an abstract class that inherits characteristics from the abstract class GasDevice.

RegulatorStation and TownBorderStation inherit attributes from GasStation.

Gas Stations house and protect pipes and devices that measure and regulate the flow of gas for the purpose of reducing higher pressures to pressures low enough to distribute to customers.

Subtypes: None

Associations: GasStructure, Regulator

Model Names: None

Attributes:

Field Name

Field Type

Description

BypassIndicator

text

Indicates whether GasStation is bypassed; domain values include Yes and No.

CPSystemStatus

text

Status of associated Cathodic Protection System.

DesignCapacityMCFH

text

Maximum amount of gas the station can manage in thousands of cubic feet per hour.

EmerIsolationSysStatus

text

Indicates whether feature defines a boundary of Emergency Isolation System; information used for tracing analysis.

GasPressureSystemStatus

text

Indicates whether feature defines a boundary of GasPressureSystem.

GasSystemStatus

text

Indicates whether feature defines a boundary of GasSystem; information used for tracing analysis.

InsulatedIndicator

text

Code indicating whether feature is insulated; domain values are Yes and No.

LocationDescription

text

Verbal description of location of the gas station.

MOPIn

double

Average maximum operating pressure entering GasStation.

MOPOut

double

Average maximum operating pressure leaving GasStation.

Name

text

Utility-assigned name of GasStation.

OverPressureProtectionType

text

Type of device to prevent overpressuring within system; domain values include Full Capacity Relief Valve, Monitor Only, Operator and Monitor, etc.

PipeDiameter

text

Code indicating size of pipe; domain values depend on subtype and include 1/4”, 1/2”, 3”, 40”, etc.

SOPIn

double

Average standard operating pressure entering GasStation.

SOPOut

double

Average standard operating pressure leaving GasStation.

Status

text

Code indicating operating status of GasStation; domain values include Offline, Online, and Unknown.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.