Warning Sign

WarningSign indicates the presence of electric lines, structures, or devices.

The WarningSign class inherits attributes from the Structure abstract class.

Subtypes: None

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

FacilityID

text

Meaningful company-assigned unique identifier.

SymbolRotation

double

Angle of rotation indicating how a feature appears on the map. Uses the SYMBOLROTATION model name. The ArcFM Manual Angle Setter edit task and ArcFM Auto Angle Setter autoupdater both use this field to rotate point features.

Directional Auto Angle Setter

double

Automatically rotates point features by the same angle of linear feature to which it is snapped, taking into account the direction the line was drawn (from point A to B, rather than point B to A). This autoupdater works only with networked features.

Endpoint Auto Angle Setter

double

Automatically rotates point features by the same angle of linear feature to which it is snapped, but flipping 180 degrees to take into account the closest line endpoint to which the point feature is snapped. This autoupdater works only with networked features.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.