TownBorderStation

A town border station is where the gas transmission system is converted to the distribution system.

This feature class has previously used the TBS model name for gas tracing. The TBS model name is no longer used but is supported for backward compatibility.

TownBorderStation inherits attributes from GasStation andGasDevice abstract classes.

Subtypes: None

Associations: Meter

Model Names: TBS

Attributes:

Field Name

Field Type

Description

PipelineOperatorNumber

text

Code indicating pipeline operator.

Supplier

text

Code indicating wholesaler from which gas is purchased.

EmerIsolationSysHighObjectID

long integer

Code indicating the emergency isolation system high side.

EmerIsolationSysLowObjectID

long integer

Code indicating the emergency isolation system low side.

GasPressureSystemHighObjectID

long integer

Code indicating the gas pressure system high side.

GasPressureSystemLowObjectID

long integer

Code indicating the gas pressure system low side.

GasSystemHighObjectID

long integer

Code indicating the gas system high side.

GasSystemLowObjectID

long integer

Code indicating the gas system low side.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.