GasSystem

GasSystem includes the components of the utility-defined hierarchy that represents the system used to deliver gas to primary utilization customers. Components include Gas Pressure Systems and Emergency Isolation Systems.

Subtypes: None

Associations: GasPressureSystem

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User and designer comments.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.