Assembly

Assembly identifies the type of structure and attachment connection.

Subtypes: None

Associations: SupportStructure

Model Names: ASSEMBLY

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

FramingType

text

Code indicating type of assembly frame; domain values include A Frame, H Frame, etc.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

StructureObjectID

long integer

ObjectID of structure supporting assembly.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.