Device Object

DeviceObject is an abstract class containing common attributes of the devices that control the flow of current in circuits. Device control objects capture characteristic strategies used by regulators and capacitors to provide voltage at a range that allows customers’ equipment to operate properly.

Associations: None

Subtypes: None

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

FacilityID

text

Meaningful company-assigned unique identifier. Many ArcFM tools use the FACILITYID model name on this field.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InstallationDate

date

Date device was installed.

Model

text

Model of the device.

SerialNumber

text

Device serial number.

WorkOrderID

text

Work order identifier.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.