Recloser Unit

Reclosers trip open a circuit for a short time to clear temporary fault and reclose after a predetermined time. The time-current characteristic, usually expressed in a curve, is based on temperature and fuse tolerances and is used to coordinate recloser operations.

Designer uses the DESIGNUNIT model name on this class to designate it as an electric device unit object class. The Designer Work Function Tool uses this model name to identify all electric device unit object classes.

Associations: Recloser

Subtypes: None

Model Names: DESIGNUNIT

Attributes:

Field Name

Field Type

Description

Manufacturer

text

Code indicating manufacturer.

RecloserObjectID

long integer

ObjectID of associated Recloser.

ReversePowerAccessory

text

Code indicating whether recloser has Reverse Power Accessory; values are Yes or No.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.