Inspection

Structures and devices are periodically inspected to ensure proper functioning and quality. The abstract class Inspection provides a way to define this information for structures, devices, controls, and units. Define specific Inspection objects on an as-needed basis. As a new Inspection object is defined, you should also define any necessary relationships.

Subtypes: None

Associations: To be defined by user

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

FacilityID

text

Meaningful company-assigned unique identifier.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InspectionDate

date

Date inspected.

InspectionType

text

Code indicating type of inspection; domain values include History, Inspection, and Maintenance.

Inspector

text

Name of inspector.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.