Service Address

Associations: CustomerConnection

Subtypes: None

Model Names: None

Attributes:

Field Name

Field Type

Description

AccountID

text

Unique identifier for the customer's account.

AcctType

text

The type of account.

Address1

text

Customer address.

Address2

text

Customer address.

Block

text

Block number of the customer's address.

City

text

Customer's city.

Comments

text

User or designer comments.

CriticalCustomerIndicator

text

Code indicating whether customer has critical need for electricity; domain values include Critical, Non-Critical.

CustomerClass

text

Code indicating class of customer; domain values include Commercial, Industrial, MultiFamily Residential, and Single Family Residential.

DesignID

text

Unique identifier for the design associated with the customer's address.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

LocationID

text

Unique identifier for the customer's location.

Lot

text

Lot number of the customer's address.

QtrSection

text

The number of the quarter section containing the service address (based on the Public Land Survey System).

Range

text

The number and direction of the range (parallel to the principal meridian, based on the Public Land Survey System) (e.g. R18E = Range 18 East).

Section_

text

The number of the section within a township (e.g. S10 = Section 10).

Situs

text

The jurisdiction where the property is treated as being located for legal purposes.

State

text

Customer's state.

StreetDir

text

Street direction in the customer's address (e.g., North, South).

StreetName

text

Street name in the customer's address.

StreetNo

text

Street number in the customer's address.

StreetSuf

text

Street suffic in the customer's address (e.g., Lane, Drive).

SubName

text

Name of the subdivision.

Township

text

Township in which the customer resides.

WorkFlowStatus

long integer

Status of the work occurring at the customer's address.

WorkFunction

long integer

The work function associated with the features (e.g., install, remove).

WorkLocationID

text

Unique identifier for the work location associated with the customer's address.

WorkRequestID

text

Unique identifier for the work request associated with the customer's address.

ZipCode

text

Customer's zip code.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.