CPRectifierCable

A rectifier cable carries power from the gas main to the rectifier and to the anode as part of the cathodic protection system. CPRectifierCable is represented as a complex edge feature because multiple connections to the network are made along its edge.

You may omit specific feature classes from gas traces. To do this, assign the GASNONTRACABLE model name to the CPRectifierCable feature class.

Subtypes: None

Associations: CPAnode

Model Names: GASNONTRACABLE

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

Depth

double

Depth of CPRectifierCable.

GasTraceWeight

long integer

Information used for tracing analysis; stored in a bitgate. Gas tracing uses the GASTRACEWEIGHT model name on this field.

Gauge

text

Code indicating gauge of cable; domain values are 4, 8, and unknown.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InstallationDate

date

Date of installation.

LengthSource

text

Source of length measurement; domain values are Mapping System and Field Measurement.

MeasuredLength

double

Field-measured length of CPSection, ranging from 1 to 1,000,000,000. Gas tracing uses the MEASUREDLENGTH model name on this field.

OperatingStatus

text

Code indicating functional status of Rectifier Cable; examples include Active, Designed, and Proposed Retire.

PropertyUnitCode

text

Value assigned to assets to track and classify Property Records.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.