Gas Field Model Names

Model Name

Object

AT_<Field Name>

Any attribute on a feature class that should be transferred from the abandoned feature class (source) when a feature is abandoned; must also exist on the appropriate field of destination feature/object class.

BONDEDINDICATOR

The attribute that indicates whether a feature is bonded; if it is bonded, it will not be a barrier to a cathodic protection trace; if it is not, it will be a barrier. Used by gas tracing.

CPSYSTEMSTATUS

The attribute that indicates whether or not a feature is a barrier to a cathodic protection trace; used by gas trace solvers.

EMERISOLATIONSYSSTATUS

The attribute on a feature that indicates whether or not it is a boundary on the emergency isolation system; used by gas trace solvers. This model name is not currently in use, but will be used in future releases.

GASPRESSURESYSTEMSTATUS

The attribute on a feature that indicates whether or not it is a boundary on the gas pressure system; used by gas trace solvers.

GASSYSTEMSTATUS

The attribute on a feature that indicates whether or not it is a boundary on the gas system; used by gas trace solvers.

GASTRACEWEIGHT

The attribute on all feature classes that represents the trace weight in the geometric network; used by gas trace solvers.

INSULATEDINDICATOR

Assign to insulated indicator field (Controllable Fitting and Non-Controllable Fitting) for gas tracing.

MATERIAL

The attribute on a feature that indicates the material of a feature to determine whether it will be a barrier to a cathodic protection trace; used by gas trace solvers.

NORMALPOSITION

The attribute on a controllable device (e.g., Valve or Controllable Fitting) that indicates whether the device is open or closed; used by gas trace solvers.

OPERATINGCLASSIFICATION

The attribute on a Valve that indicates whether the valve is critical (see the Operating Classification domain for possible values); used by gas trace solvers.

OPERATINGPRESSURE

The attribute on the DistributionMain feature class that indicates the operating pressure of the pipe.

PIPEDIAMETER

The attribute on a gas pipe that indicates its diameter.

PIPESTATUSINDICATOR

The attribute on a gas pipe that indicates whether the pipe is pinched or damaged in some way, such that gas will not flow through it; used by gas trace solvers.

PIPETYPE

The attribute on a gas pipe that indicates whether the pipe is a pinchable type (see the Pipe Type domain for possible values); used by gas trace solvers.

SOPIN

Attribute on RegulatorStation that indicates standard or system operating pressure entering station; used by gas trace solvers.

SOPOUT

Attribute on RegulatorStation that indicates standard or system operating pressure leaving station; used by gas trace solvers.

STATUS

Assign to the Status field on Regular and Town Border Station features; used by gas trac e solvers.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.