Electric Field Model Names

Model Name

Object

ACTUALDUCTSIZE

ActualDuctSize attribute in DuctDefinition object (optional)

AT_<Field Name>

Any attribute of a source feature class that should be transferred to the abandoned (destination) feature class; must also exist on the corresponding field of the destination feature/object class

CLASS

Assign to attribute that represents class of structure; used for structural analysis

CIRCUITSOURCEGLOBALID

Assign to the GlobalID field in CircuitSourceID tables. This field and field model name enable Extended Feeder Manager to use Global IDs.

CIRCUITSOURCEGUID

Assign to the GUID field added to any table except the CircuitSourceID table. This field and field model name enable Extended Feeder Manager to use GUIIDs.

IMPORTANT: Do NOT assign this to the CircuitSourceID table.

CIRCUITSOURCEID

Assign to the CircuitSourceID field. This field and field model name are used by Feeder Manager to support multi-tiered networks.

CONDUCTORMATERIAL

Assign to attribute of ConductorInfo or overhead conductor feature class that represents material of conductor; used for structural analysis

CONDUCTORSIZE

Assign to attribute of ConductorInfo or overhead conductor feature class that represents size of conductor; used for structural analysis

DEVICETYPE

Indicates the type of device. Assigned to the DeviceType field on the MMENG_DEVICEWEIGHT field for Structural Analysis (Designer only).

DIAMETER

The attribute on any overhead support structure feature class that represents the diameter of the structure; used for structural analysis

DUCTAVAILABILITY

Available attribute in DuctDefinition object

DUCTBANKCONFIGURATION

DuctBankConfiguration attribute in conduit feature class with ULS model name

DUCTBANKHEIGHT

Height attribute in DuctDefinition object (optional)

DUCTBANKWIDTH

Width attribute in DuctDefinition object (optional)

DUCTID

DuctID attribute in DuctDefinition object (optional)

DUCTMATERIAL

Material attribute in DuctDefinition object

DUCTNAME

Name attribute on the Duct feature class

DUCTOCCUPIED

Occupied field on the Duct feature class

DUCTSIZE

DuctSize attribute in DuctDefinition object

FACILITYDIAGRAM

FacilityDiagram field on the UndergroundStructure feature class

FACILITYID

Assign to FacilityID field of Transformer feature class; used by Secondary Circuit Analysis

FDRMGRGANGOPERATED

Indicates whether a device is gang operated.

FDRMGRNONTRACEABLE

The attribute on any feature class that indicates whether a feature should be traced by Feeder Manager.

For a detailed explanation of FDRMGRNONTRACEABLE, view the appendix help topic: Appendix > Bitgate Fields > Electric Tracing - Edges.

FEEDERID

The FeederID field in any network listed as part of a feeder; also the FeederID field in the CircuitSource object

FEEDERID2

The FeederID2 field in any network listed as part of a feeder

FEEDERINFO

The FeederInfo field in any network feature listed as part of a feeder

FEEDERLEVEL

Assign to the FeederLevel field. This field and field model name are used by Feeder Manager to support multi-tiered networks.

FEEDERNAME

The FeederName in the CircuitSource object.

FEEDERSOURCEINFO

The FeederSourceInfo field in the CircuitSource object

GROUNDREACTANCE

Ground reactance field of Transformer

GR0UNDRESISTANCE

Ground resistance field of Transformer

GUYCOUNT

Assign to attribute on AnchorGuy feature class that represents the number of guys in the system; used for structural analysis

HASSUBDUCTS

HasSubducts field on the Duct feature class

HEIGHT

Assign to attribute on AnchorGuy feature class that represents the height of the structure; used for structural analysis

HIGHSIDECONFIGURATION

Assign to HighSideConfiguration field of Transformer

HIGHSIDEGROUNDREACTANCE

Assign to HighSideGroundReactance field of Transformer

HIGHSIDEGROUNDRESISTANCE

Assign to HighSideGroundResistance field of Transformer

INSULATIONTYPE

Assign to insulation type field

JOINTATTACHMENTOWNER

Assign to the Owner field of the JointUseAttachment table

LASSOTEXT

The LassoText field in the Lasso feature class (ULS/contents relate tool)

LASSOTEXTFIELD

Assign to field that is source for a different label than label in the contents list of cross section annotation feature for a conductor or cable feature class contained in a conduit system

LEADLENGTH

Assign to lead length field

LOWSIDECONFIGURATION

Assign to LowSideConfiguration field of Transformer

LOWSIDEGROUNDREACTANCE

Assign to LowSideGroundReactance field of Transformer

LOWSIDEGROUNDRESISTANCE

Assign to LowSideGroundResistance field of Transformer

LOWSIDEVOLTAGE

Assign to LowSideVoltage field of Transformer

MANUFACTURERMODEL

Assign to the Manufacturer Model field in the MMENG_DEVICEWEIGHT table for Structural Analysis. Designer only.

MATERIAL

Assign to attribute on overhead support structure feature class that represents the material; used for structural analysis

MMELECTRICTRACEWEIGHT

Assign to electric trace weight field of features participating in Feeder Manager and electric trace tasks

MMSECCKTAMPACITY

Assign to Ampacity field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis

MMSECCKTCODE

Assign to Code field of MMENG_TRANSFORMER and MMENG_CONDUCTOR_ELEC tables; used for secondary circuit analysis

MMSECCKTCOST

Assign to Cost field of MMENG_TRANSFORMER and MMENG_CONDUCTOR_ELEC tables; used for secondary circuit analysis

MMSECCKTCUCODE

Assign to CUCode field of MMENG_TRANSFORMER and MMENG_CONDUCTOR_ELEC tables; used for secondary circuit analysis

MMSECCKTDESCRIPTION

Assign to Description field of MMENG_TRANSFORMER and MMENG_CONDUCTOR_ELEC tables; used for secondary circuit analysis

MMSECCKTINSULATION

Assign to Insulation field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis

MMSECCKTMATERIAL

Assign to Material field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis

MMSECCKTR_PER1000UNITSLENGTH

Assign to R_Per1000_Units_Length field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis

MMSECCKTR0_PER1000UNITSLENGTH

Assign to R0_Per1000_Units_Length field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis

MMSECCKTSIZE

Assign to CondSize field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis

MMSECCKTTRANSFORMERFULLLOADLOSSMAX

Assign to FULL_LOAD_LOSS_MAX field of MMENG_TRANSFORMER table; used for secondary circuit analysis

MMSECCKTTRANSFORMERNOLOADLOSSMIN

Assign to FULL_LOAD_LOSS_MIN field of MMENG_TRANSFORMER table; used for secondary circuit analysis

MMSECCKTTRANSFORMERKVA

Assign to kVA field of MMENG_TRANSFORMER table; used for secondary circuit analysis

MMSECCKTTRANSFORMERMAXXTOR

Assign to X_TO_R_MAX field of MMENG_TRANSFORMER table; used for secondary circuit analysis

MMSECCKTTRANSFORMERMAXZ

Assign to Percent_Z_MAX field of MMENG_TRANSFORMER table; used for secondary circuit analysis

MMSECCKTTRANSFORMERMINXTOR

Assign to X_TO_R_MIN field of MMENG_TRANSFORMER table; used for secondary circuit analysis

MMSECCKTTRANSFORMERMINZ

Assign to Percent_Z_MIN field of MMENG_TRANSFORMER table; used for secondary circuit analysis

MMSECCKTTRANSFORMERNOLOADLOSSMAX

Assign to NOLOAD_LOSS_MAX field of MMENG_TRANSFORMER table; used for secondary circuit analysis

MMSECCKTTRANSFORMERNOLOADLOSSMIN

Assign to NOLOAD_LOSS_MIN field of MMENG_TRANSFORMER table; used for secondary circuit analysis

MMSECCKTTRANSFORMERPHASES

Assign to Phasing field of MMENG_TRANSFORMER table; used for secondary circuit analysis

MMSECCKTUNDERGROUND

Assign to Underground field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis

MMSECCKTX_PER1000UNITSLENGTH

Assign to X_Per1000_Units_Length field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis

MMSECCKTX0_PER1000UNITSLENGTH

Assign to X0_Per1000_Units_Length field of MMENG_CONDUCTOR_ELEC table; used for secondary circuit analysis

NEUTRALMATERIAL

Assign to attribute on overhead support structure feature class that represents the material of neutral cable; used for structural analysis

NEUTRALSIZE

Assign to attribute on overhead support structure feature class that represents the size of the neutral cable; used for structural analysis

NOMINALVOLTAGE

Used by the ArcFM Inherit Nominal Voltage autoupdater. Assign to the Nominal Voltage field on the Primary Conductor and Transformer feature classes.

NORMALPOSITION_A

The attribute on all switchable feature classes (e.g., fuse, switch) that indicates the position (open or closed) of phase A

NORMALPOSITION_B

The attribute on all switchable feature classes (e.g., fuse, switch) that indicates the position (open or closed) of phase B

NORMALPOSITION_C

The attribute on all switchable feature classes (e.g., fuse, switch) that indicates the position (open or closed) of phase C

NUMBERCONDUCTORSPERPHASE

Assign to attribute on ConductorInfo or overhead conductor feature class that represents the number of conductors present for each phase; used for structural analysis

OPERATINGVOLTAGE

The attribute on any conductor feature class or bus bar feature class that indicates the operating voltage of the feature

PARENTCIRCUITSOURCEGUID

Assign to the GUID field added to any table, including any CircuitSourceID table, that had the field model name PARENTCIRCUITSOURCEID assigned to a field. Used by Extended Feeder Manager to support the use of GlobalIDs.

PARENTCIRCUITSOURCEID

Assign to the ParentCircuitSourceID field. This field and field model name are used by Feeder Manager to support multi-tiered networks.

PHASEDESIGNATION

The attribute on any Conduit System member that indicates the phase of the feature (to support Conduit System Management); the attribute on any transformer feature class or load point feature class (e.g., PrimaryMeter) that indicates the phase of the feature (to support Feeder Manager); the attribute on any conductor that indicates the phase of the conductor (to support the Auto Phase Assign autoupdater)

RATEDKVA

The RatedKVA field in the DistributionTransformer feature class and the TransformerUnit object

RATING

Assign to the Rating field in the MMENG_DEVICEWEIGHT table for Structural Analysis. Designer only.

RELATEDFEATURECLASSNAME

Assign to the RelatedFeatureClassName field. This field and field model name are used by Feeder Manager to support multi-tiered networks.

RELATEDOBJECTID

Assign to the RelatedObjectID field. This field and field model name are used by Feeder Manager to support multi-tiered networks.

SERIALNUMBER

Assign to the Serial Number field in the MMENG_DEVICEWEIGHT table for Structural Analysis. Designer only.

SERVICECURRENTRATING

Assign to service current rating field; used by secondary circuit analysis

SUBSOURCE

Assign to the SubSource field. This field and field model name are used by Feeder Manager to support multi-tiered networks.

SUBSTATIONID

The SubstationID field in the CircuitSource object

SUBTYPECD

The field on the Duct Definition object class that indicates the subtypes defined

ULSTEXTFIELD

In a ULSMember, designates field used for display in Cross Section contents list (optional)

USAGETYPE

The attribute on any overhead support structure feature class that represents the type of use of the structure; used for structural analysis

WIRESIZE

Assign to attribute on AnchorGuy that represents the guy wire size; used for structural analysis

WIRESTRENGTH

Assign to attribute on AnchorGuy that represents the guy wire strength classification; used for structural analysis

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.