CrossingInspection

CrossingInspection represents a point at which inspections occur for locations where pipe crosses streams or other bodies of water or other obstacles such as railroad lines, highways, etc.

Subtypes: None

Associations: Drip, LeakReport, PipeExposure

Model Names: None

Attributes:

Comments: text -User or designer comments.

DistributionMainObjectID: long integer -ObjectID of associated Distribution Main.

Hyperlink: text -Used to store a hyperlink path via standard Esri hyperlinking functionality.

Inspector: text -Name of Inspector for previous inspection.

LastInspectionDate: date -Date of last inspection.

LocationDescription: text -Verbal description of location.

NextInspectionDate: date -Date of next inspection.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.